Chassis information view parameters

Chassis information
view includes these parameters:
TIP: These parameters are available when the project is online.
Parameter
Description
Slot
Displays the number of the configured slot. Valid values are 1…32.
Base Catalog
Displays the mounting base catalog number.
Base Status
Displays the status of the mounting base. Valid values:
  • Faulted
  • OK
Details
Opens the Basexx details dialog which contains mounting base identification and diagnostics.
IO Catalog
Displays the I/O catalog number.
Field Power
Displays whether field power is present.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal