Basexx details parameters

Basexx details
includes these parameters:
Parameter
Description
Recommended Actions
Vendor
Displays the mounting base vendor name.
Product Type
Displays the type of product.
Product Name
Displays the mounting base name.
Catalog Number
Displays the mounting base catalog number.
Series
Displays the mounting base catalog number series.
Revision
Displays the firmware revision.
CIP Serial Number
Displays the CIP serial number.
Manufacture Date
Displays the manufactured date.
Serial/Warranty Number
Displays the serial/warranty number.
Fault Exists
Displays whether a base fault is present.
IO Module
Displays whether an I/O module is present.
IO Module Not Detected Timestamp
Displays the fault timestamp when a module is not detected.
Field Power
Displays whether there is field power present.
Field Power Off Timestamp
Displays the field power off timestamp when present.
Internal Fault
Displays whether there is an internal fault present.
Cycle power to the entire chassis. If the fault persists, replace the mounting base. If the fault still persists, replace the adapter.
Internal Fault Timestamp
Displays the internal fault timestamp when present.
Authentication Fault
Displays whether there is an authentication fault present.
Return the I/O module. Contact Rockwell Automation Technical Support.
Revision Fault
Displays whether there is a revision fault present.
If there is no authentication fault present, reset or power cycle the adapter. If the fault persists, update the adapter to the latest firmware revision.
Revision/Authentication Fault Timestamp
Displays the fault timestamp when a revision or authentication fault is detected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal