Servers view parameters
TIP:
These parameters are available only when the application is online.
Disabling the server while using the Protection Mode decreases the possibility of a
security breach.
Parameter | Description |
|---|---|
Enable | Enables or disables the server by selecting or clearing the checkbox. |
Name | Indicates the name of the server. |
Port | Indicates the port number of the server. |
Protocol | Indicates the protocol used by the server. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Writes pending edits to the device. Set is available only when there are pending edits. |
Provide Feedback