Disabling HTTPS and SNMP servers interrupts access to device web pages and SNMP
clients
Selecting
Set
in the Servers
view writes
changes to the device. If you disable the SNMP and HTTPS servers and select
Set
, it interrupts access to the SNMP clients and the device web
pages.Verify that an interruption now is acceptable, and then select
Yes
to
apply the changes. Select No
to cancel the operation.Provide Feedback