Disabling the HTTP server interrupts access to device web pages

Selecting
Set
in the
Servers
view writes changes to the device. If you disable the HTTP server and select
Set
, it interrupts access to the device web pages.
Verify that an interruption now is acceptable, and then select
Yes
to apply the changes. Select
No
to cancel the operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal