Overview view parameters
Parameter | Description |
|---|---|
Series | Displays the series of the device. |
Revision | Displays the major and minor revisions of the device. |
Electronic keying | Displays the electronic keying used for the device as Exact
Match , Compatible Module , or Disable
Keying . Electronic keying compares the device defined in the project
to the installed device. If keying fails, a fault occurs. |
Channel Mode Assignment | Displays the Channel Mode Assignment method used for the device. Possible values
include:
Predefined with Generic IO-Link is only available when you
select Major Revision 3 in the Device Definition dialog. If you select Major
Revision 1 or 2, then User-Selectable is the only method for
Channel Mode Assignment. |
Connection | Displays the connection format for the device. |
Device definition | Opens the dialog to change the device-specific parameters. |
Parameter | Description |
|---|---|
Ch XX | Indicates the individual channel to which the operation mode applies to. |
<Selected Mode> | Displays the selected operation mode for the channel. |
Provide Feedback