Output parameters
The Output parameters apply to the following channel mode types:
- Output
- IO-Link, Input Output, Timestamp
- Input Output, Timestmap
- IO-Link (Generic), Input Output, Timestamp
- IO-Link (Generic), Input Output
The Output parameters include:
Parameter | Description |
|---|---|
Output State in Program Mode Program state | Determines the value to which output changes when the device transitions to Program
mode. |
Output State in Communication Fault Mode Communication fault state | Determines the value to which output changes when the device transitions to
Connection Fault mode. |
Output State in Communication Fault Mode Communication fault state duration | Determines the length of time the Fault Value value is held prior to the Final
Fault State. |
Output State in Communication Fault Mode Final communication fault state | Determines the value to which the output changes if these events exist:
|
Output State When Communication Fails in Program Mode | Determines output action if a connection faults while the device is in Program
mode. The output can remain as Output State in Program mode or transition to Output State
in Communication Fault mode. When the output remains as Output State in Program mode, the Final Fault State is
ignored. |
Enable No Load diagnostics | Determines whether the No Load detection is enabled. When the No Load detection is
used, if a wire is disconnected from an output that is turned off (No Load
condition), the I.Ptxx.NoLoad member goes to 1. This parameter is not available when the channel mode is set to Digital
Output, Group Short Circuit or Digital Output, Short
Circuit . |
Diagnostics | Opens the diagnostics dialog to view diagnostic information. |
Provide Feedback