IO-Link parameters

The IO-Link parameters apply to the following channel mode types:
  • IO-Link
  • IO-Link, Input Output, Timestamp
The IO-Link parameters include:
Parameter
Description
Disable channel
Disables the channel by selecting the checkbox.
When the channel is disabled, both IO-Link communication and Digital Input on the channel are deactivated.
Diagnostics
Opens the diagnostics dialog to view diagnostic information.
IO-Link port event log
Opens the XX – IO-Link Port Event Log dialog to view diagnostic information.
Disable and delete Data Storage
Disables Data Storage and deletes the master copy of the Data Storage on this port.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal