XX Diagnostics - Output dialog parameters
Parameter | Description | Value |
|---|---|---|
Fault exists | Shows whether a fault is present on the connected device. |
|
Data uncertain | Reserved | No |
Short circuit fault | Shows whether the channel has a short circuit or overcurrent
fault. |
|
LA power fault | Shows whether the channel has a LA Power fault. |
|
No load fault | Shows whether the channel has a No Load fault. |
|
Last fault timestamp | Shows the timestamp of the last fault in
YYYY -MM -DD -HH :mm :SS .mmm
format.
| A valid time or None if no event time is recorded. |
Provide Feedback