XX Diagnostics - IO-Link dialog parameters
Parameter | Description | Value |
|---|---|---|
IO-Link status | Shows the status of the connected device. |
|
Fault exists | Shows whether a fault is present on the connected device. |
|
Data uncertain | This bit is only set when the LA Power Fault or LA Power Short Circuit
bit is set. |
|
CQ short circuit fault | Shows whether the channel has a a CQ short circuit or overcurrent
fault. |
|
SA power fault | Shows whether the channel has a Sensor Actuator Power fault. |
|
SA power short circuit fault | Shows whether the channel Sensor Actuator Power has a short circuit or
overcurrent fault. |
|
LA power fault | Shows whether the channel has a Local Actuator Power fault. This parameter only applies when IO-Link Class B Power is
enabled. |
|
LA power short circuit fault | Shows whether the channel Local Actuator Power has a short circuit or
overcurrent fault. This parameter only applies when IO-Link Class B Power is
enabled. |
|
Last fault timestamp | Shows the timestamp of the last fault in
YYYY -MM -DD -HH :mm :SS .mmm
format.
| A valid time or None if no event time is recorded. |
Provide Feedback