XX Diagnostics - Input, Fallback dialog parameters
Parameter | Description | Value |
|---|---|---|
IO-Link status | Shows the status of the connected device. |
|
Fault exists | Shows whether a fault is present on the connected device. |
|
Data uncertain | Reserved | No |
CQ short circuit fault | Shows whether the channel has a a CQ short circuit or overcurrent
fault. |
|
SA power fault | Shows whether the channel has a Sensor Actuator Power fault. |
|
SA power short circuit fault | Shows whether the channel Sensor Actuator Power has a short circuit or
overcurrent fault. |
|
Last fault timestamp | Shows the timestamp of the last fault in
YYYY -MM -DD -HH :mm :SS .mmm
format.
| A valid time or None if no event time is recorded. |
Provide Feedback