Device Diagnostics dialog parameters
Parameter | Description | Value |
|---|---|---|
Run mode | Shows the operating state for the device. Run Mode is blank when the application is
offline, or when the connection is not established to the
device. |
|
Diagnostics thresholds exceeded | Shows whether any diagnostic threshold has been reached when the
event occurred. |
|
Diagnostics sequence count | Shows the count for each time a distinct diagnostic condition was
detected, and also each time a distinct diagnostic condition
transitioned from detected to not detected. | 0…255 |
Self test | Shows whether the product initialization code detected an error. |
|
CPU utilization | Shows the usage of the compute engine. | 0…100% |
Connections | Shows the number of open CIP connections open. | 0…32,767 |
Packets lost | Shows the running sum of the number of Sequenced Address Item
Sequence Numbers that are skipped in Class 0 and Class 1 connections
consumed by the device. | 0…2,147,483,647 |
Timeouts | Shows the running count of the number of connections that time out,
both originated and targeted, to the device. | 0…2,147,483,647 |
HMI packet rate | Shows the number of Class 3 packets and unconnected packets sent and
received by the device in the previous second. | 0…2,147,483,647 |
IO packet rate | Shows the number of Class 0 and Class 1 packets that were transmitted
or received by the device in the previous second. | 0…2,147,483,647 |
Ethernet errors | Shows the sum over all ports of these Ethernet Link object
values:
| 0…2,147,483,647 |
Time Synchronization Status | Shows whether the device is synchronized with an IEEE 1588 master
clock. |
|
Time Synchronization Grand master clock identity | Shows the identity of the grandmaster clock to which the device is
synced. | 8-byte hex number |
Time Synchronization Local clock offset to system time | Shows the offset, in nanoseconds, from the local clock to the system
time. Use this value to detect steps in time. This value updates when a
Precision Time Protocol (PTP) update message is received. | -9,223,372,036,854,775,808 …+9,223,372,036,854,775,807 |
Time Synchronization Local clock offset timestamp | Shows the timestamp of the local clock offset in
YYYY-MM-DD-HH:mm:SS.mmm format.
| A valid time or None if no event time is recorded. |
SA Power Fault | Shows whether the device has a Sensor Actuator Power fault. |
|
LA Power Fault | Shows whether the device has a Local Actuator Power fault. |
|
Internal fault | Shows whether the device has an internal fault. |
|
SA Power Fault Timestamp LA Power Fault Timestamp Internal fault timestamp | Shows the timestamp of the last fault in
YYYY -MM -DD -HH :mm :SS .mmm
format.
| A valid time or None if no event time is recorded. |
Provide Feedback