Fallback

When a channel operation mode is set to
Fallback
:
  • You can configure the device through the IO-Link interface.
  • The device operates in the Digital Input or Digital Input, Timestamp mode.
The Digital Input data or Digital Input, Timestamp data is available in the IO-Link master device input tag for this channel.
You can fall back the device to the
Digital Input
, or
Digital Input, Timestamp
mode by uninhibiting the IO-Link device attached to this channel.
You can wake up the device to IO-Link mode by inhibiting the IO-Link device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal