Channel Assignments view parameters
You can configure the parameters only when Channel Mode Assignment is configured as
User-Selectable
.
TIP:
When Channel Mode Assignment is configured as
Predefined with Generic IO-Link
, the selected mode for
each channel is fixed and cannot be changed.Parameter | Description |
|---|---|
Port | Displays the device port number from 0…7. |
Channel | Displays the device channel number from 0…15. |
Selected Mode | Specifies the operation mode for the channel. Possible values for channels 0, 2, 4, 6, 8, 10, 12, and 14
include:
Possible values for channels 1, 3, 9, and 11 include:
Possible values for channels 5, 7, 13, and 15 include:
|
Available Modes | Indicates the available mode types for the channel.
|
Provide Feedback