Connection with Events invalid
No compatible channel mode configured for the "Data with Events" or "Data with Events and
Status" connection type.
The compatible modes are:
- Digital Input
- Digital Input, Timestamp
- Digital Input, Counter
- Digital Input, Fallback
- Digital Input, Timestamp, Fallback
- IO-Link, Digital Input Output, Timestamp
- Digital Input Output, Timestamp,
Configure at least one channel as an input or counter and apply the changes.
Provide Feedback