Confirm Device Definition changes
Confirm any changes that are being made to the module’s definition.
- Yes = SelectYesto update the appropriate values and return to Overview. Data is recovered from existing settings or set to their default values, as appropriate. Configurations are updated, as required for the new device definition.At this point, the changes have not been applied to the Studio 5000 Logix Designer application project and only exist within the scope of the profileAlso note that you must selectApplyto commit the changes to the Studio 5000 Logix Designer application project. This provides the opportunity to review the changed data and make adjustments as required prior to committing the changes to the module.
- No = SelectNoto return to Overview without changing any values.
Provide Feedback