Channel xx Mode invalid

When an IO-Link device exists on the channel, the channel mode cannot be changed:
  • From "IO-Link" or "IO-Link, Digital Input Output, Timestamp" to "Digital Input, Fallback" or "Digital Input, Timestamp, Fallback". OR
  • From "Digital Input, Fallback" or "Digital Input, Timestamp, Fallback" to "IO-Link" or "IO-Link, Digital Input Output, Timestamp". OR
  • From "IO-Link", "IO-Link, Digital Input Output, Timestamp", "Digital Input, Fallback", or "Digital Input, Timestamp, Fallback" to any other channel modes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal