Counter parameters

The Counter parameters apply to the following channel mode types:
  • Counter
The Counter parameters include:
Parameter
Description
Off → On filter time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
On → Off filter time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Preset
Displays the value set in the Output tag O.Counterxx.Preset member to use for counter preset.
Rollover at preset
Causes the counter to rollover to 0 at the Preset value.
Diagnostics
Opens the diagnostics dialog to view diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal