Channels view parameters
If Channel Assignment Mode is configured as
User-Selectable
, the
following parameters are displayed.Parameter | Description |
|---|---|
Disabled channels | Displays the channel whose mode is set to Disabled .This parameter is not available if there are no disabled channels. |
Power Supply channels | Displays the channel whose mode is set to Power Supply .This parameter is not available if there are no Power Supply channels. |
Port | Displays the device port number from 0…7. |
Channel | Displays the device channel number from 00…15. |
Mode | Displays the operation mode for the channel. |
Output State During Program Mode | Determines output channel action when the controller transitions to Program
mode. Valid values are:
|
Output State During Communication Fault Mode | Determines output channel action when a connection fault occurs. Valid values are:
|
Input Filter Time Off → On | Specifies a value by which to delay the transition from Off to On. This delay is
useful for filtering out transients in noisy environments. The associated memebers are:
Valid values are:
|
Input Filter Time On → Off | Specifies a value by which to delay the transition from On to Off. This delay is
useful for filtering out transients in noisy environments. The associated memebers are:
Valid values are:
|
Counter Preset | Displays the value of the Output tag O.Counter xx .Preset member
to use for counter preset. Valid values are from 0…2,147,483,647 μs. |
Counter Rollover at Preset | Causes the counter to rollover to 0 at the Preset value by selecting the
checkbox. The associated member is C.Counterxx.RolloverAtPreset, whose valid values are:
This parameter is shaded when the mode is set to anything other than
Digital Input, Counter . |
Diagnostics | Opens the diagnostics dialog to view diagnostic information. This parameter is shaded when the device is offline or the mode is set to one of
these values:
|
If Channel Assignment Mode is configured as
Predefined with Generic
IO-Link
, the following parameters are displayed.Parameter | Description |
|---|---|
Port | Displays the device port number from 0…7. |
Channel | Displays the device channel number from 00…15. |
Mode | Displays the operation mode for the channel. |
Output State During Program Mode | Determines output channel action when the controller transitions to Program
mode. Valid values are:
|
Output State During Communication Fault Mode | Determines output channel action when a connection fault occurs. Valid values are:
|
Input Filter Time Off → On | Specifies a value by which to delay the transition from Off to On. This delay is
useful for filtering out transients in noisy environments. The associated memebers are:
Valid values are:
|
Input Filter Time On → Off | Specifies a value by which to delay the transition from On to Off. This delay is
useful for filtering out transients in noisy environments. The associated memebers are:
Valid values are:
|
Diagnostics | Opens the diagnostics dialog to view diagnostic information. This parameter is shaded when the device is offline. |
Provide Feedback