Points view parameters (output)
The
Points
view includes these parameters:Parameter | Description |
|---|---|
Output State During | Determines the output points behavior in the Program and Fault mode. |
| Determines each output's behavior when the controller transitions to the Program mode. The available values are:
While in the Program mode, outputs from the controller are ignored and the output behaves according to one of the above. |
| Determines the output points behavior after a communication fault occurs and the device enters the Communications Fault mode. The available values are:
|
Fault Mode Output State | Determines how the output point transitions from the Fault mode. |
| Indicates the time the output remains in the Fault mode before transitioning to the final state. The available values are:
|
| Determines whether the device transitions to an On or Off state after the Fault mode duration time elapses. The default final state is Off. If you choose Forever for Duration , you cannot choose a final state. The device retains its current Fault mode state. |
Electronic Fuse | Sends a Reset Fuse message to the device for the appropriate point. |
When Communication Fails in Program Mode | Sets the result of a communication failure in the Program mode:
|
Provide Feedback