Inputs view parameters
The
Inputs
view includes these parameters:Parameter | Description |
|---|---|
Hardware Input Ties | Assigns counter control functions for individual counters to hardware inputs. Configure the setting for each counter by choosing from the available parameters.
|
Up/Down | Causes a counter to increment or decrement accumulated count or changes the direction bit for frequency values.
|
Count Enable | Acts as a gate input that controls when counting starts and stops.
|
Reset Count | Resets the count to zero.
|
Preset Count | Determines the starting value for a count. Each counter can have one preset value.
|
Provide Feedback