CounterX view parameters
The
CounterX
view includes these parameters:Parameter | Description |
|---|---|
Calculate Average Frequency Over | Indicates the number of pulses for calculating average frequency. Valid values = 0…1,000 Default = 10 |
Frequency Calculation Timeout | Defines the maximum time in milliseconds(ms) the counter waits before calculating frequency if the number of pulses specified in Calculate Average Frequency Over were not received.Valid values = 0…10,000 ms Default = 1,000 ms |
Enable Filter of this Counter | Select this checkbox to enable filtering on an individual point. |
Window 0 Defined in | Defines the method that Window 0 uses to evaluate incoming pulses. Methods available:
|
Window 1 Defined in | Defines the method that Window 1 uses to evaluate incoming pulses. Methods available:
|
Input Tie Configuration | Displays information about the hardware input tie configuration settings.
|
Provide Feedback