Counters view parameters
The
Counters
view includes these parameters:Parameter | Description |
|---|---|
Counter | Identifies the counter inputs. |
Calculate Average Frequency Over | Indicates the number of pulses to use for calculating average frequency (0 … 1000). |
Frequency Calculation Timeout | Indicates the time in milliseconds to wait before the counter calculates frequency (0 … 10000 ms). |
Window 0 Defined in | Defines the method Window 0 uses to evaluate incoming pulses. Methods available:
|
Window 1 Defined in | Defines the method Window 1 uses to evaluate incoming pulses. Methods available:
|
Enable Filter | Enables or disables filtering. When filtering is enabled, transitions at a counter input point must remain in the new state for a configured length of time before the device begins counting. Configure the filter time in the Inputs view. |
Provide Feedback