Calibration view parameters
The
Calibration
view includes these parameters:
IMPORTANT:
Entering calibration mode causes all input channels to freeze at their current values and fault. Control may be impaired.
Parameter | Description |
|---|---|
Channel | Displays the channel to which this configuration applies. |
Calibration Range | Displays the range in which the channel will be calibrated based on the current device selected. Calibration Range may also be fixed or dependent on the Input Range selected during configuration. |
Calibration Gain | Displays the calibration gain correction factor currently being applied to the channel. |
Calibration Offset (Counts) | Displays the calibration offset correction factor in DAC/ADC counts currently being applied to the channel. |
Calibration Status | Indicates if the existing calibration for the channel is considered bad. A calibration is considered bad if:
|
Start Calibration | Starts the calibration process. If you are using the 1756-OF4 or 1756-OF8 devices for current or voltage applications, select the appropriate Output Range or Input Range in the Configuration view.Available only when the controller is online. |
Last Calibration Date | Displays the date on which the device was last successfully calibrated. |
Provide Feedback