ChX ramp value must be greater than zero
One of these error conditions occurs:
Condition | Solution |
|---|---|
ChX ramp rate value is less than 0. | Enter a value greater than 0. |
ChX rate limit value is less than 0. | Enter a value greater than 0. |
Provide Feedback