ChX alarm value is too low
One of these conditions occurs:
Condition | Solution |
|---|---|
ChX high limit value is less than the low limit value. | Enter a high limit value greater than the low limit value. |
ChX high limit value is less than the low low limit value | Enter a high limit value greater than the low low limit value |
ChX high high limit value is less than the low limit value | Enter a high high limit value greater than the low limit value. |
ChX high high limit value is less than the low low limit value. | Enter a high high limit value greater than the low low limit value. |
Provide Feedback