Time Synchronization view parameters
Parameter | Description |
|---|---|
UTC system time | Indicates the current system time in Universal Coordinated Time (UTC). The time does not include time zone or daylight savings time offsets. |
Grandmaster Clock | Indicates property information for the grandmaster clock. |
Identity | Displays the unique identifier for the clock. |
Local Clock | Indicates property information for the local clock. |
Synchronization status | Specifies whether the local clock is synchronized or not synchronized with the grandmaster reference clock. |
Provide Feedback