Fault/Program Action view parameters (1732E-8CFGM8R, 1732E-16CFGM12R)

Parameter
Description
Points
Indicates the points to which the configuration applies.
Output State During
Program Mode
Specifies the behavior of each output when the controller's mode changes to Program. Valid values are:
  • Off
    (default)
  • On
  • Hold
This parameter is not available in Run mode.
Output State During
Fault Mode
Specifies the behavior of each output when the connection from the controller to the output device is broken. Valid values are:
  • Off
    (default)
  • On
  • Hold
This parameter is not available in Run mode.
WARNING:
Turning on Program Mode or Fault Mode applies output voltage to all self-configured points, regardless of whether the point is used as an input or an output.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal