Invalid engineering value

The high engineering value equals to the low engineering value.
The high or low engineering value is the value used in the Data input tag when the analog signal is at the value specified for
High Signal
or
Low Signal
. The default value for
High Engineering
is 100.0000 and for
Low Engineering
is 0.0000. The valid range is from -1.0E+11 through 1.0E+11.
Enter appropriate engineering values and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal