Voltage Register Map

This register map contains parameters that are used to Line and Tune Voltages in RMS, the voltage in these parameters described by a factor of 10, meaning that a value of 10 indicates 1.0 Vrms. Note that some parameters shown below may not exist in the parameter database/ or shown in PQvision. These parameters have been reserved for future use and are enabled in EtherNet/IP EDS File.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
6
: Voltage Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet Name)
Instance ID
Description
Type
Default & Ranges
Notes
V_LINE_AB_RMS (VLineABRMS)
219
Line voltage phase AB RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Source Utility Line Phase to Phase Voltage (A-B)
V_LINE_BC_RMS (VLineBCRMS)
220
Line voltage phase BC RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Source Utility Line Phase to Phase Voltage (B-C)
V_LINE_CA_RMS (VLineCARMS)
221
Line voltage phase CA RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Source Utility Line Phase to Phase Voltage (C-A)
V_LOAD_AB_RMS (VLoadABRMS)
234
Load voltage phase AB RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Filter Output Phase to Phase Voltage (A-B)
V_LOAD_BC_RMS (VLoadBCRMS)
235
Load voltage phase BC RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Filter Output Phase to Phase Voltage (B-C)
V_LOAD_CA_RMS (VLoadCARMS)
236
Load voltage phase CA RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Filter Output Phase to Phase Voltage (C-A)
V_TUNE_A_RMS (VTuneABRMS)
246
Tuned circuit voltage phase AB RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
V_TUNE_B_RMS (VTuneBCRMS)
247
Tuned circuit voltage phase BC RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
V_TUNE_C_RMS (VTuneCARMS)
248
Tuned circuit voltage phase CA RMS,
(10 = 1.0 Volts)
R
Default:0
Range: 0 to 1000 Vrms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal