Data
The following module data types and tags are created by the AOP:
- Input Tags
- Channel values
- Status and Fault words
- Timestamps
- Output Tags
- Configuration Tags - configurable through the AOP configuration tabs
Note
: IO Tags are updated by the controller asynchronous to its ladder-logic program scan. When "block integrity" of this data is important, the CPS ladder instruction can synchronously copy the data to other tags for use by application logic. Refer to the "User’s Guide" for recommended methods.Provide Feedback