Sample Projects
Locating the Sample Projects
Example ladder logic may be available as a RSLogix5000 or Studio5000 Sample Project file for ControlLogix. Please check the SLP85xD Documentation website at www.mt.com/SLP85xD, or the RA sample code download website at Sample Code Download
Using the Sample Projects
Sample Projects can be used as a model for a separate application, as the start for a new project, or by copying or importing elements to another project. RSLogix5000/Studio5000 partial Import/Export can be used to add a sample project to an existing application project. This minimizes the number of user steps involved, and provides automatic checking and handling of conflicts with the existing project (e.g. duplicate tag names, etc.). Refer to RA publication 1756-RM084K-EN-P, "Logix5000 Controllers Import/Export Reference Manual”, available for download at the Rockwell Automation website (www.rockwellautomation.com).
Provide Feedback