Sample Projects

The IND570 Terminal PLC Interface Manual and the IND570 Documentation CD contains RSLogix5000 ladder logic examples describing the steps involved in Reading and Writing data to the TAG and creating the CIP Data Table Read and Write message instructions required to read data from and write data into the IND570 Terminal EtherNet/IP Interface Read and Write TAG Data Tables.
Locating the Sample Projects
The example ladder logic may be available as a RSLogix5000 Sample Project file for ControlLogix. Or it may be available as an Add-On Instruction (AOI). Please check the IND570 Documentation CD (P/N # 30205330), or the RA sample code download website at Sample Code Download
Using the Sample Projects
Sample Projects can be used as a model for a separate application, as the start for a new project, or by copying or importing elements to another project. RSLogix5000 partial Import/Export can be used to add a sample project to an existing application project. This minimizes the number of user steps involved, and provides automatic checking and handling of conflicts with the existing project (e.g. duplicate tag names, etc.). Refer to RA publication 1756-RM084K-EN-P, "Logix5000 Controllers Import/Export Reference Manual”, available for download at the Rockwell Automation website (www.rockwellautomation.com).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal