Documentation
Manual
The primary source for detailed information about the unit is the manual that came with the unit and Remote Access Control manual. Both of these manuals can be downloaded from www.pentairprotect.com.
EDS File
The EDS file is used for identifying the module to network tools, such as RSLogix5000 and RSLinx. The EDS file can be downloaded from www.pentairprotect.com and installed using the RSLinx Hardware Installation Tool.
EtherNet_IP Objects File
The EtherNet_IP Objects file identifies the objects supported, Assembly Instance size and Requested Packet Interval. The file can be downloaded from www.pentairprotect.com.
Provide Feedback