Scale Calibration

Use the Scale Calibration view to calibrate the scale module.
  • Perform a C2 calibration
  • Search for connected C2 devices
  • Perform "Hard" calibration with reference and span test weights
IMPORTANT: C2 devices are detected on power up. If C2 devices have been connected after power up, run a C2 Search prior to a C2 Calibration.
TIP: This page communicates directly with the device and is not available if the device or the project is offline.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal