Integrated Technician

Use this page to run INTEGRATED TECHNICIAN tests and view the test status and outcome.
  • Perform an INTEGRATED TECHNICIAN test, if you have no Hardy IT JBOX
  • Perform an INTEGRATED TECHNICIAN test with a Hardy IT JBOX, with 1, 2, 3, or 4 load cells attached
If you do not have a Hardy IT JBOX, you can view the excitation sense voltage, which should be close to the voltage at the load cells, typically around 5 volts.
You can also view the combined weight, which is the weight on the load cells, and the combined mv/v, which should equal the voltage on the load cell signal lines divided by the excitation voltage.
The "internal reference" is a referenced signal produced internally on the HI5069-xWS.
If you have a Hardy IT JBOX, you can also view the weights and mv/v values on up to 4 separate load cell inputs.
TIP: This page communicates directly with the device and is not available if the device or the project is offline.
TIP: The HI5069-xWS Owner’s Guide, which is available online by following the hyperlink on the
Vendor Information
tab, provides additional information for the parameters discussed in this help file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal