Overview View
Use the Overview view to view the definition of a device, including the device type,
revision, electronic keying, connection, and other device-specific values.
TIP:
To change the definition of a device, select
Device definition
in the Overview view.The Overview view includes these parameters.
Parameter | Description |
|---|---|
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the
device defined in the project to the installed device. If keying fails, a fault
occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems
Application Technique, publication LOGIX-AT001 . |
Connection Type | Displays the type of IO connection configured to the module. |
Device definition | Opens Device definition to change the revision, electronic
keying, and Connection Count values. |
Provide Feedback