Live Data and Status
Use the Live Data and Status view to display live weight and status information from the
scale module.
- View the gross weight, or ZERO the gross weight
- View the net weight, or TARE
- View the status of the scale
TIP:
This page communicates directly with the device and
is not available if the device or the project is offline.
Provide Feedback