Integrated Technician
Use this page to run INTEGRATED TECHNICIAN tests and view the test outcome.
- Perform an INTEGRATED TECHNICIAN test, if you have no Hardy IT JBOX
- Perform an INTEGRATED TECHNICIAN test with a Hardy IT JBOX, with 1, 2, 3, or 4 load cells attached
If you do not have a Hardy IT JBOX, you can view the excitation sense voltage, which should
be close to the voltage at the load cells, typically around 5 volts.
If you have a Hardy IT JBOX, you can also view the weights and mv/v values on up to 4
separate load cell inputs.
TIP:
This page communicates directly with the device and
is not available if the device or the project is offline.
TIP:
The HI5034-WS Owner’s Guide, which is available
online by following the hyperlink on the
Vendor Information
tab,
provides additional information for the parameters discussed in this help file.Provide Feedback