Connection View

Use the Connection view to specify controller-to-device connection configuration.
  • Select a requested packet interval.
  • Choose to inhibit the device connection(s).
  • Configure the controller so that a loss of connection to this device causes a major fault in the controller.
  • Enable or disable publishing of diagnostics to FactoryTalk Alarms and Events.
  • View connection faults.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal