Configuration
Add-On-Profile (AOP)
The module functionality is configured through a custom, separately-installable
Add-on-Profile within Studio 5000 Logix Designer Software. When a module from the Logix
Designer Select Module dialog is added to the project tree, the following items are created
in the project:
- A custom Module-Defined Data Type, and corresponding Input, Output Tags
- A producer/consumer IO connection using the module’s specific IO assemblies and sizes
DIP Switches for Hardware Addressing
The IP address of the measuring device can be configured for the EtherNet/IP network using
the DIP switches. Addresses in the range from 0 to 254 are permitted (the address 255 is
reserved for the broadcast address). The IP address for software addressing is active when
the device leaves the factory (default IP address: 192.168.1.212), i.e. all the DIP switches
for hardware addressing are set to OFF. Switches 1-8 configure the last three digits (last
octet) of the IP address. The first three octets can be configured via software addressing
to reflect the desired hardware IP address.
Setting the IP address with switches

Provide Feedback