Empty Pipe Detection

Empty Pipe Detection

Activate or deactivate detection of an empty or partially filled pipe.
TIP: Due to low density, deactivate partially filled pipe detection for a gas.
Empty Pipe Detection parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Switch Point Empty Pipe Detection

Enter hysteresis in % below which the measuring tube will be detected as empty.
Switch Point Empty Pipe Detection parameter properties
Property
Value
Selection / Range
0 - 100 %
Factory Setting
50 %
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT

Response Time Empty Pipe Detection

Enter the time before diagnostic message "S862 Pipe empty" is displayed for empty pipe detection
Response Time Empty Pipe Detection parameter properties
Property
Value
Selection / Range
0 - 100 s
Factory Setting
1 s
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT

New Pipe Empty/Full Adjustment

Select empty pipe or full pipe adjustment to perform a new adjustment. To adjust empty pipe detection, perform the empty pipe adjustment first and then the full pipe adjustment.
TIP: The measuring device is pre-adjusted at production using water (approx. 300 μS/cm). For liquids that deviate from this conductivity, a new empty pipe and full pipe adjustment must be performed on site.
New Pipe Empty/Full Adjustment parameter properties
Property
Value
Selection / Range
  • Cancel
  • Empty pipe adjust
  • Full pipe adjust
Factory Setting
Cancel
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Adjustment Progress

Shows the progress of the process.
Adjustment Progress parameter properties
Property
Value
Selection / Range
  • Ok
  • Busy
  • Not Ok
Factory Setting
Not Ok
Visibility
Operator
Write Access
Read-Only
Data Type
ENUM16

Current Empty Pipe Detection Measured Value

Displays the value currently measured for empty pipe detection.
Empty Pipe Detection Measured Value parameter properties
Property
Value
Selection / Range
0 - 3.4E+38 Ohm
Factory Setting
0 Ohm
Visibility
Operator
Write Access
Read-Only
Data Type
FLOAT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal