Error & Warning Limits

A monitoring of process values can be activated for:
  • Volume flow
  • Liquid Temperature
  • Liquid velocity
  • Volume totalizer 1 & 2
  • Differentiation factor
  • Acoustic transmission factor
  • Density
  • Mass flow
  • Mass totalizer 1 & 2
  • Concentration 1 & 2
A monitored value can be:
  • in the normal operating range
  • in the warning range (Namur state: “Check Function”)
  • in the error range (Namur state: “Failure”)
You can set 4 limit values: 2 error limits and 2 warning limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal