Calibration
If the FLOWave needs to be adjusted, the following process values can be adjusted to
compensate for certain installation or process specificities. For example, a reduced inlet
section can compensate for a flow error by adjusting the k factor.
Flow calibration should be done after the density calibration if required.
Possible process values for calibration:
- Volume flow
- Temperature
- Differentiation factor
- Acoustic transmission factor
- Density
Provide Feedback