Concentration
Damping
The damping makes it possible to damp the fluctuations of the measured values of the liquid
concentration:
- On the display.
- On the PLC inputs.
The damping is not applied to the new measured value if the 2 following conditions are met:
- A Low, Medium or High damping level is active.
- The measured value changes by more than 30% of full scale.
Provide Feedback