Confirm the changes to the definition of a device

Use the settings in
Apply changes
to confirm any changes that are being made to the device’s definition.
  • In
    Apply changes
    , select
    Yes
    to update the appropriate values.
Data is recovered from the previous definition's settings or set to their default values, as appropriate. Configurations are updated, as required for the new device definition.
TIP:
The changes are not applied to the software project and only exist within the scope of the profile. To make the changes to the project, select
OK
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal