Overview view parameters
The
Overview
view includes these parameters.
TIP:
The available parameters in the
Overview
view are based on the
device being configured. Parameters that do not apply to the device are hidden.Parameter | Description |
|---|---|
Series | Displays the device series. |
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Connection | Displays the Connection Type and the Communication Format. |
Rack Connection | Displays the connection to communicate with the I/O devices in the remote chassis.
Valid values include:
|
Input Data / Output Data | Displays the input or output data type for the device. |
Data Format | Displays the type of data transferred between the device and controller. |
Counters | Displays the counter number for the device. |
Chassis size | Displays the chassis size of the device. |
Configured by | Displays the entity that configures the device. |
Muting Lamp Points | Displays the muting lamp points for the device. |
Device definition | Opens Device definition to change the revision, electronic keying, and other device specific values. |
Safety Network Number | Enter a 48-bit number to prevent the acceptance of connection requests that have been misdirected by an intervening bridge device. Safety devices connected to the same bridge device need not be on the same safety network; they may have different safety network numbers. Choose from the following two formats.
This field appears shaded in the Run, Safety Locked, and Safety Signature modes. |
Provide Feedback