Invalid Beacon Interval or Beacon Timeout value
The device cannot support the current Beacon Interval or Beacon Timeout. The device cannot
support either the Beacon Interval or Beacon Timeout values of the current Active
Supervisor.
Enter a Beacon Interval and a Beacon Timeout value within the supported range for the device.
Check the user manual for the correct range for the device. Apply the changes.
Provide Feedback