Disabled all active ports. At least one active port must remain enabled at all times.
You attempted to disable all active ports. For devices with three or more ports, you can
safely disable multiple ports, but the system does not allow you to disable the
last
active
port. Disabling the last active port does not allow communication device
recovery without a physical reset or reconfiguration.Provide Feedback