FactoryTalk® Design Studio™ is a new cloud-based software product built from the ground up to improve system design efficiency. Available anytime, anywhere using only a web browser, there are no downloads or installs required and no software maintenance responsibility.
Beginning with controller design, FactoryTalk Design Studio reduces development time by leveraging modern software development practices and an integrated version control system. Teams can collaborate more easily than ever with automated tools to share and merge changes and project sizes can scale dynamically with support for multiple controllers in a single project. FactoryTalk Design Studio is ready to change the way industrial automation systems are created.
FactoryTalk Design Studio is one of the five core solutions in FactoryTalk® Design Hub™. Industrial organizations can now transform their automation design capabilities with a more simplified, productive way to work powered by the cloud. Teams of all sizes, skillsets and locations can work smarter through enhanced collaboration, improved lifecycle management and on-demand access to cloud-based software all while adhering to the latest security standards and information technology (IT) best practices. The result is increased design productivity, faster time to market and systems that cost less to build and maintain.
Published February 9, 2023